Create a rectangle or square object
Use the rectangle tool to draw rectangles and squares.
TIP:
Squares and rectangles are specialized polygons, so the Properties dialog boxes are the same as for the polygon object.
To create a rectangle or square object
- In theGraphics Displayeditor, selectObject > Drawing > Rectangleor drag
from the toolbox. - Press the mouse button, drag the mouse diagonally to draw the object to the desired size, and release the button.TIP:PressCtrlas you drag the mouse to draw a square.
- Double-click the object to open itsPropertiesdialog box.
- In thePropertiesdialog box, specify how you want the rectangle to look.
- ClickOK.
Provide Feedback