Numeric pop-up scratchpad keys
The following table shows the keys on an external keyboard or keypad.
Keys | Descriptions |
|---|---|
Decimal | The decimal button (.) on an external keyboard or keypad works only if the decimal point type is Implicit. |
Minus | Press the minus key on an external keyboard or keypad to toggle the value between positive and negative. |
Escape | To close the pop-up scratchpad without writing the value to the Value connection, press the ESC key on an external keyboard or keypad |
Backspace | Press on an external keyboard or keypad to delete the right-most digit. Hold the button down to delete multiple digits. If there are no digits left in the scratchpad, the minus sign, if any, is removed. |
Enter | Press on an external keyboard or keypad to write the value to the Value connection. |
Delete | Press the Delete key on an external keyboard or keypad to clear the scratchpad. |
Provide Feedback
on an external keyboard or keypad to delete the right-most digit. Hold the button down to delete multiple digits. If there are no digits left in the scratchpad, the minus sign, if any, is removed.
on an external keyboard or keypad to write the value to the Value connection.