Create Numeric Input Enable buttons
At runtime, the operator can use the
Numeric Input Enable
button to open a numeric pop-up keypad or scratchpad. When the operator presses the button, the pop-up opens. The operator can use the pop-up to enter a numeric value to send to the Value connection at the data source,
or to ramp a displayed value up or down.To create a Numeric Input Enable button
- In theGraphics Displayeditor, selectObjects > Numeric and String > Numeric Input Enableor drag
from the toolbox. - Drag the mouse to position and draw a rectangle the general size and location you want the button to be.
- Double-click the button to open itsPropertiesdialog box.
- In thePropertiesdialog box, specify how the button looks and how it will work at runtime.
Provide Feedback