Options on the Alarm tab of the Alarm Status List Properties dialog box
The following table shows the options on the
Alarm
tab of the Alarm Status List Properties
dialog box.Options | Descriptions |
|---|---|
Column | Specify which columns to use, their width, and header text, if any. |
Display header | Select this check box to show column headers on the object. |
Display title | Select this check box to show the title of the list. |
Select a column | Select a column to be edited:
|
Display column | Select this check box if you want the selected column to appear on the object. |
Width | Type the width in pixels of the selected column. |
Header text | Type the text to show for the header of the selected column. |
List settings | Select how many lines each alarm can use, and word wrap behavior for messages. |
Lines per alarm | Select the number of lines, from 1 to 10, each alarm will occupy in the object. The default is 1. |
Word wrap | Select this check box if you want the text to continue on the next line at the beginning of a new word. If this check box is cleared, the text continues on the next line whenever the maximum text length is reached, even if this occurs in the middle of a word or number. The maximum text length depends on the width of the object and the font size. |
List Mode | Select whether to show all alarms, currently active alarms, or alarms that have been active in the past. |
All Alarms | All the alarms that have been set up in the Alarm Setup editor, whether they are active, inactive, or never have been active, will be shown. |
Active alarms | Only currently active alarms are shown. When an alarm becomes inactive, it is removed from the list. |
Past alarms | Alarms that have been active at some point since the last reset are shown, whether they are currently active. |
Titles | Use the default title for the selected list, or type a title up to 80 characters long. |
Filtering | Filter the object to show only the alarms from the specified triggers. |
Filtered triggers | Click the Browse button to open the Trigger Label Selector, where you can select the alarm trigger labels whose alarms will be included on the display as they occur.If this box is blank, all alarms are shown. |
Provide Feedback