Create an alarm status list
You may need to create an alarm status list on a graphic display.
To create an alarm status list
- In theGraphics Displayeditor, selectObjects > Advanced > Alarm > Alarm Status Listor drag
from the toolbox. - Drag the mouse to position and draw a rectangle the general size and location you want the list to be.
- Double-click the list to open itsPropertiesdialog box.
- In thePropertiesdialog box, specify how the list looks.
Provide Feedback