Options on the Print tab of the Print Alarm Status Button Properties dialog box
The following table shows the options on the
Print
tab of the Print Alarm Status Button Properties
dialog box.Options | Descriptions |
|---|---|
Column | |
Select a column | By default, all the columns in the alarm status display are selected for printing. If you want to omit a column or columns from the print, select the column and clear the Print check box.
|
Print | Check this box for each column that you want to print. Clear this box for each column that you do not want to print. |
Width | Type the number of characters for the width of the selected column. This property applies only to the Trigger label and Trigger value columns. |
Heading | |
Title | Type a title for the printed report, up to 80 characters long. The default title is Alarm Status. |
Print type | |
All Alarms | Select to print the status of all the alarms set up in the Alarm Setup editor. |
Active alarms | Select to print the status of only those alarms that are currently active. |
Past alarms | Select to print the status of all the alarms that have been active since the alarm status was last reset. |
Provide Feedback