Create an Alarm button
All Alarm buttons are created in the same way.
To create an Alarm button
- In theGraphics Displayeditor, selectObjects > Advanced > Alarmand then select the button you want to create, or drag the icon from the toolbox:
- Acknowledge Alarm

- Acknowledge All

- Alarm Status Mode

- Clear Alarm Banner

- Clear Alarm History

- Print Alarm History

- Print Alarm Status

- Reset Alarm Status

- Silence

- Sort Alarms

- Drag the mouse to draw a rectangle of the general size and in the general location you want the button to be.
- Double-click the button to open itsPropertiesdialog box.
- In thePropertiesdialog box, specify how the button looks.
Provide Feedback