Options on the General tab of the Alarm Banner Properties dialog box
The following table shows the options on the
General
tab of the Alarm Banner Properties
dialog box.Options | Descriptions |
|---|---|
Appearance | Specify the object's appearance in this area. |
Border style | Select a border style for the object. |
Border width | Type the number of pixels for the width of the object’s border. |
Back style | Specifies the object background. Available options are:
|
Pattern style | Select a pattern for the object. The pattern appears on the face of the object. The pattern does not cover the object’s border or alarms. If the object’s back style is transparent or gradient, the pattern is not visible. |
Border uses back color | Select this check box to use the object’s background color for the border of the object. Clear this check box to use the selected Border Color . |
Back color | This box shows the current background color for the object. Click it to select another color. If the background style is transparent, the application does not use this background color. If the background style is gradient, click it to bring up the Gradient Fill dialog box to configure the gradient fill. |
Border color | This box shows the border color for the object. Click it to select another color. If Border uses back color is not selected, this color appears at runtime. |
Pattern color | This box shows the current pattern color for the object. Click it to select another color. |
Fore color | This box shows the color of the text shown on the object. Click it to select another color. If Use alarm colors is selected, the application does not use this color. Instead, it shows messages using the Foreground and Background colors defined on the Messages tab of the Alarm Setup editor. |
Use alarm colors | Select this check box to show alarm messages using the Background and Foreground colors defined in the Alarm Setup editor instead of the Fore color and Back color selections on this tab. |
Blink | Select this check box if you want the alarm message to blink at runtime. The blink rate is twice per second. |
Text | The text properties apply to the alarm messages in the alarm banner. |
Font | Select the font to use for the message. |
Size | Select the font size to use for the message. |
Bold, Italic, Underline | Select a font style for the message, if required. |
Word wrap | Select this check box if you want the text to continue on the next line at the beginning of a new word. If this check box is cleared, the text continues on the next line whenever the maximum text length is reached, even if this occurs in the middle of a word or number. The maximum text length depends on the width of the object and the font size. |
Alignment | Select how you want the text to be positioned on the object. |
Other | |
Key navigation | Select this check box to allow the user to navigate to the object using the keyboard and give the object input focus. |
Use Alarm Identifier | Select this check box to write the alarm identifier value assigned to the alarm message to the tag specified for the AlarmIdentifier connection. |
Provide Feedback