Create an alarm banner
You may need to create an alarm banner on a graphic display.
To create an alarm banner
- In theGraphics Displayeditor, selectObjects > Advanced > Alarm > Alarm Banneror drag
from the toolbox. - Drag the mouse to position and draw a rectangle the general size and location you want the banner to be.
- Double-click the banner to open itsPropertiesdialog box.
- In thePropertiesdialog box, specify how the banner looks.
Provide Feedback