Options on the General tab of the Maintained Push Button Properties dialog box
The following table shows the options on the
General
tab of the Maintained Push Button Properties
dialog box.Options | Descriptions |
|---|---|
Appearance | Specify the object's appearance in this area. |
Border style | Select a border style for the object. If the object shape is circle or ellipse, the available border styles are None and Line . |
Border width | Type the number of pixels for the width of the object’s border. |
Back style | Specifies the object background. Available options are:
Specify the color for the background ( Back color ) on the States tab. |
Shape | Select the shape of the object. If the object shape is circle or ellipse, the application applies properties such as size and position by measuring in relation to the object’s bounding box. |
Border uses back color | Select this check box to use the object’s background color for the border of the object. Clear this check box to use the selected Border Color .Specify the background color and the border color on the States tab. |
Highlight color | This box shows the current highlight color. Click it to select another color. The object's border, if any, changes to the highlight color when the operator presses the button at runtime. |
State settings | |
Next state based on | Select how the button changes states:
If the value does not match one of the button’s state values, the application changes the button to State 0 and writes out the State 0 value. |
Touch margins | You can specify a touch-insensitive margin inside the button’s edges. If the operator presses on the touch-insensitive margin, the button press is not registered. |
Horizontal margin | Specifies the number of pixels for the distance inside the left and right edges of the button where the button will not be touch sensitive. |
Vertical margin | Type the number of pixels for the vertical touch margin. The vertical margin is along the button’s top and bottom edges. |
Other | |
Audio | Select this check box to sound an internal beeper when the object is pressed. If the computer running the project does not have an internal beeper, the object press does not trigger a beep. |
Provide Feedback