Create a Maintained push button
Use the Maintained push button object to create a button that toggles between two values. This type of button is useful for changing a setting within a machine or process, but not for starting the machine or process.
A Maintained push button sends one value to the data source the first time it is pressed, and a second value the next time it is pressed and released.
IMPORTANT:
Do not use push buttons for emergency stops. Emergency stop buttons must be hard-wired.
To create a Maintained push button
- In theGraphics Displayeditor, selectObjects > Push Button > Maintainedor drag
from the toolbox. - Drag the mouse to position and draw a rectangle the general size and location you want the button to be.
- Double-click the button to open itsPropertiesdialog box.
- In thePropertiesdialog box, specify how the button looks, how to change states, and its tags.
Provide Feedback