Linear Gauge Properties - General tab
The following table shows options under
Appearance
of the General
tab.Options | Description |
|---|---|
Border style | Select the border style for the object. |
Border width | Enter the number of pixels for the width of the object’s border. |
Back style | Select whether the object background is solid, gradient, or
transparent.
|
Gauge style | Select a gauge style from the list:
|
Value indicator | Select the size of the value indicator. |
Alarm indicator | Select whether to show the alarm indicator or the size of the alarm
indicator. It is displayed when the current value reaches or crosses
a threshold. |
Border uses back color | Select this check box to use the object’s background color for the
border. If this is not selected, you can assign a separate color to
the border, instead of using the object’s background color. |
Back color | This field displays the current background color for the object.
Click it to select another color.
Solid , the
background color is used for the spaces between the dots or
dashes. |
Border color | This field displays the border color for the object. Click it to
select another color. This color appears at runtime only if
Border uses back color is not selected. |
Value indicator color | This field displays the current color of the value indicator, which
is a triangle on the side of the linear gauge. Click it to select
another color.
TIP:
The value indicator color determines the line color of
the sparkline.
|
The following table shows options under
Scale settings
of the General
tab.Options | Description |
|---|---|
Outline color | Select the color for the linear gauge's scale outline and ticks. |
Show ticks | Select this check box to show the ticks on the linear gauge. |
Major ticks | Select the number of major ticks.
TIP:
The number of major ticks on the scale
determines the number of grid lines in the sparkline: horizontal grid lines if the gauge
is vertical, and vertical grid lines if the gauge is horizontal.
|
Minor ticks | Select the number of minor ticks. |
Show legend | Select this check box to show the legend on the major ticks. |
Field length | Select the character length of the tick legend. |
Decimal places | Select the number of digits to show after the decimal point. |
Font and Size | Select the font type and size for the tick legend. |
Provide Feedback