Options in the Gradient Fill dialog box
The following table shows the options in the
Gradient Fill
dialog box.Options | Descriptions |
|---|---|
Colors | Move the slider to change the percentage of the start and end color. |
Start color | Click the Start color box to choose the start color for the gradient fill. |
End color | Click the End color box to choose the end color for the gradient fill. |
Horizontal | Click Horizontal to make the color gradient in a horizontal direction. |
Vertical | Click Vertical to make the color gradient in a vertical direction. |
Diagonal Up | Click Diagonal Up to make the color gradient in a diagonal up direction. |
Diagonal Down | Click Diagonal Down to make the color gradient in a diagonal down direction. |
Styles | A linear gradient color is specified by two points, and a color (or different intensity of one color) at each point. Depending on the points' positions, there are four styles you can select. |
IMPORTANT:
The
PanelView Plus 7
and PanelView Plus 6
terminals cannot process a Gradient Fill that uses a Diagonal Up or Diagonal Down direction, nor can the terminal apply a Gradient Fill to a rotated object. When running an MER on a PanelView Plus 7
or PanelView Plus 6
terminal and the system encounters an object with these attributes, the system shall use the gradient fill starting color as the object's solid color background.When running the MER on a computer, the system can process all gradient fills and this warning does not apply.
Provide Feedback