Keys with predetermined functions
The following table shows the keys with predetermined functions.
Keys | Descriptions |
|---|---|
Page Right | Press this key to switch to the next defined key set. If no next key set is defined, pressing Page Right has no effect. |
Page Left | Press this key to switch to the previous defined key set. If no previous key set is defined, pressing Page Left has no effect. |
Home | Press this key to load the first defined key set. |
Provide Feedback