Connections for the Custom String Popup Keyboard ActiveX control
The following table shows the connections to control the operation of the Custom String Popup Keyboard ActiveX control at runtime.
Connections | Descriptions |
|---|---|
Value Required | The configured tag contains the user-entered string returned by the control. The connection is write-only and can be a memory or direct reference tag. The connection data type is String. |
Launch Enable Required | When the configured tag transitions from zero (0) to non-zero, the keyboard will be shown to the user. The connection is read-only and can be a memory or direct reference tag. The connection data type is Analog. |
Provide Feedback