Options in the Insert an ActiveX Control dialog box
The following table shows the options in the
Insert an ActiveX Control
dialog box.Options | Descriptions |
|---|---|
Register | Click the Register button to register an ActiveX control to the system registry and show the control in the Insert an ActiveX Control dialog box. |
Unregister | Click the Unregister button to remove the selected ActiveX control from the system registry and the Insert an ActiveX Control dialog box. |
Provide Feedback