Add an ActiveX control to a graphic display
You may need to add an ActiveX control to a graphic display.
To add an ActiveX control to a graphic display
- InFactoryTalk View Studio, selectObjects > ActiveX Controlor drag
from the toolbox. - On the graphic display, drag the ActiveX tool to draw a rectangle the size you want the object to be.
- In theInsert an ActiveX Controldialog box, select the object you want to add and clickOK.The object is placed on the display. Depending on how the third party implemented the object, it might be a different size than the rectangle you drew.
- To specify the object’s properties and assign tags or expressions to its connections, do one of the following:
- Right-click the object, and then selectPropertiesto open the object’sPropertiesdialog box.Depending on how the third party implemented the object, it might not have aPropertiesdialog box. If thePropertiesmenu item is not available, use the next method.
- Right-click the object and selectProperty Panel.
- In thePropertiesdialog box orPropertiestab of theProperty Panel, specify the object’s properties.
- (Optional) Set up the properties on theCommontab.
- On theConnectionstab, assign tags or expressions to the object’s connections.
- ClickOKto close thePropertiesdialog box, or clickCloseto close theProperty Panel.
TIP:
- If an ActiveX control you have installed does not appear in theInsert an ActiveX Controldialog box, the object might not be registered. Register the control using theInsert an ActiveX Controldialog box before you can add it to a graphic display.
- To define the properties for an ActiveX control, you can double-click the object to open itsPropertiesdialog box or right-click the object and selectProperty Panelto make the changes.
- You can attach visibility animation to an ActiveX control by assigning a tag or expression to the object in theAnimationdialog box.
- Configure your video adapter to show more than 256 colors to make sure that the colors of the ActiveX controls appear the same as in the original.
Provide Feedback