Configure NFC

Configure NFC for compatible CIP Secure devices.
IMPORTANT: Devices newly added to the policy model always have NFC disabled.
Prerequisites
Log on to
FactoryTalk Policy Manager
as an administrator. See Log on to FactoryTalk Policy Manager.
  1. To configure NFC
  2. Add NFC-compatible CIP Secure devices. See Add a device.
  3. Configure NFC device properties. See Device properties | NFC.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal