NFC
Configure the Near Field Communication (NFC) permissions for data exchange with
supported devices added to the security policy model.
TIP:
You cannot configure NFC for devices in the
Onboarding Area. For more information, see Onboarding.
Configuration
FactoryTalk Policy Manager
administrators can configure NFC settings for compatible
CIP Secure devices. See Configure NFCStatuses
NFC statuses include:
- Disabled.Do not allow devices that are not in the security policy model to read from or write to the device through NFC.
- Read-only.Allow devices that are not in the security policy model to read from the device through NFC.
- Read and write.Allow devices that are not in the security policy model to read from or write to the device through NFC.
IMPORTANT:
Devices newly added to the policy model always have
NFC disabled.
Provide Feedback