Reset a node
Reset the configuration of a node device to factory defaults.
- Select the gateway device that contains the node device to reset.
- SelectCanvasand then select a device.
- SelectZonesand then select a zone and a device.
- SelectDevicesand then select a device.
- InPROPERTIES, next to the node to reset, select.
Reset device configuration to factory defaults - IMPORTANT: Resetting device configuration to factory defaults is irreversible.InReset device configuration to factory defaults, selectReset configuration.
A message displays and informs about the successful reset operation.
Provide Feedback