EtherNet in Cabinet
Use gateways to securely add EtherNet/IP smart devices such as contactors or push
buttons to the security policy model.
For more information, search for EtherNet in Cabinet in Literature Library.
Gateways
Gateways introduce additional policies to configure the nodes connected to the gateway.
Gateways share security settings with all associated nodes.
You can add gateways to zones as secure devices, either manually or through the automatic
device discovery. For more information, see Configure automatic device discovery or Add a device.
To remove a gateway, remove all associated nodes first.
Replace a gateway in the same manner as other devices. For more information, see Replace a device.
Nodes
Nodes are EtherNet/IP smart devices associated with gateways. To add nodes to the security
policy model, add an associated gateway device to the security policy model and then refresh
the nodes list. Each gateway supports up to 39 nodes.
Manage nodes by:
- Adding nodes to gateways. See Add nodes to a gateway.TIP: Nodes are not listed in theTablesandCanvasviews.
- Replacing individual node devices connected to gateways. See Replace a device.
- Resetting node device configurations to factory defaults. See Reset a node.
Conduits
You can only create unidirectional conduits to gateways. The communication always flows
from gateways to other conduit endpoints. You cannot create conduits that link directly to
nodes.
CIP Security profile
CIP Security
profile describes which security features a given device
supports. Devices enforce security policies based on security profiles. For more
information, refer to CIP Security with Rockwell Automation Products
,
publication SECURE-AT001D-EN
.Property | Description |
|---|---|
Transport | DTLS |
Authentication | Nodes use pre-shared keys (PSKs) to authenticate communication with gateways.
PSKs for gateways and all associated nodes are the same. |
Cryptographic algorithms | AES-GCM, ChaCha20-Poly1305, SHA-256 |
Provide Feedback