Conduits

Conduits are communication pathways in the policy model, connecting pairs of policy model components.
You can create conduits between these components:
CIP conduits
Endpoint 1
Endpoint 2
Zone
Zone
Zone
Device
Zone
Range
Device
Device
Device
Range
OPC UA conduits
Endpoint 1
Endpoint 2
Zone
Zone
Zone
OPC UA
server
Zone
OPC UA
client
Zone
Range
OPC UA
client
OPC UA
server
Conduits must follow these rules:
  • Conduits cannot be duplicated, each combination of endpoints must be unique.
  • One of the endpoints must be
    CIP Security
    or
    OPC UA security policy
    capable.
  • If one endpoint is a zone, the other endpoint cannot be a device within that zone.
  • Devices not assigned to any zone or onboarding devices cannot be used as endpoints.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal