Devices table
Manage devices to add, edit, replace, and delete devices.
Devices table interface

Item | Name | Description |
|---|---|---|
![]() | Table | Lists all devices in the policy model, unassigned devices, and devices to be deleted from the policy model. IP addresses of device ranges are delimited with a hyphen . IP addresses of redundant controllers are delimited with a comma . Controllers configured as redundant systems appear as a single device in the security policy model. Select not grayed-out table cells to edit values. Select a table header title to sort elements based on the column values. Drag a table header to change the order of columns in the table. Filter tables by hovering-over a table header, selecting |
Item | Description |
|---|---|
Add Device | Adds a device to the selected zone. |
Add Range | Adds a range to the selected zone. |
Replace Device | Replaces the selected device. |
Delete | Deletes the selected device. |
Clear Filters | Clears all filters. |
Filter | Filters table rows based on the specific criteria. See Filter tables. |
Provide Feedback