Discovery pane

Use the
Discovery
pane to browse discovered devices and
OPC UA
servers and their endpoints, configure networks, and manage drivers.
TIP: To open or close the
Discovery
pane, select
Discovery
from the right toolbar.

CIP

Toolbar
Item
Description
Add
Add
Adds selected CIP devices to the selected zone.
Auto browse
Continuously discover CIP devices and networks.
Zoom in
Increases the size of the network topology tree.
Zoom out
Decreases the size of the network topology tree.
Search
Toggles
Search
that provides a filtered list of devices based upon the specified search criteria.
Advanced Settings
Opens advanced network settings.
Configure Drivers
Adds a driver on the computer to provide communications to a network and configures existing drivers for edit or delete.
Show CIP Security Indicators
Show or hide the
CIP Security
configuration status of a device.
CIP Security indicators
Indicator
Description
Gray shield icon
The device supports
CIP Security
and is not yet configured.
Orange shield icon with an exclamation mark
The device is in the
CIP Security
configuration process.
Green shield icon with a check mark
The device is successfully configured with
CIP Security
.
Yellow shield icon with a quotation mark
The device is not recognized.
Red shield icon with a cross mark
The device configuration process encountered an error.
(no indicator icon)
The device does not support
CIP Security
.

OPC UA

Toolbar
Item
Description
Add
Add
Adds selected
OPC UA
devices to the selected zone.
Auto browse
Verify manually added
OPC UA
servers and their connection endpoints in the policy model.
Advanced Settings
Opens advanced network settings.
Discover OPC UA Server
Opens a dialog that enables you to add an
OPC UA
server and discover its connection endpoints.
Filter
Provides a filtered list of devices based on the filter query.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal