Save Canvas to a graphic file

Save the policy model visualization to a graphic file.
  1. From the navigation bar, select
    Canvas
    .
  2. From the toolbar, select
    Save
    .
  3. Select any of the following:
    • Save entire canvas
      . Saves the entire policy model visualization.
    • Save only visible portion of canvas
      . Saves the policy model visualization that is currently visible in the
      FactoryTalk Policy Manager
      window.
  4. Select
    Save
    .
  5. Navigate to the location to save the file and select
    Save
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal