Graphical Explorer
Use
Graphical Explorer
to browse the zones, devices, and conduits tree. You can filter, collapse, and expand the tree nodes.
TIP:
Selecting a component in the
Graphical Explorer
tree focuses the policy model visualization on that component. Selecting a component in the policy model visualization, focuses the tree on that component.You can expand or collapse the
Graphical Explorer
pane.Item | Description |
|---|---|
Filter | Filter tree based on specific criteria. Filtering the policy model tree does not impact items displayed on
canvas. For more information, see Filter Graphical Explorer. |
Zones | Zones added to the policy model and devices added to these zones. |
Conduits | Conduits added to the policy model. |
Onboarding Area | Devices found by Automatic Policy Deployment that can be added to the policy
model. |
Unassigned | Devices that are added to the policy model but are not added to any zone in the
policy model. |
Hide | Collapse Graphical Explorer . |
Show | Expand Graphical Explorer . |
Provide Feedback