Change Canvas layout
Change how the policy model representation is displayed.
- From the navigation bar, selectCanvas.
- To change the layout:
- Move a zone container. Select, hold, and move the zone header.
- Collapse or expand a zone container. In the zone header selector
.
- Display conduits as curved lines. From the toolbar, selectCurved Lines.
- Display conduits as straight lines. From the toolbar, selectStraight Lines.
- Distribute containers automatically. From the toolbar, selectAuto Layout.
Provide Feedback