Writing material phase logic

Writing phase logic for a material phase requires some additional consideration. The
FactoryTalk Batch
Server requires that a simple protocol be followed by the phase logic programmer to ensure that inventory levels are properly maintained within the material database and that the
FactoryTalk Batch
Event Journal contains entries identifying the inventory that was produced or consumed.
Protocol:
  • The phase logic must request a download of the AMOUNT parameter.
  • Before entering a terminal state (COMPLETE, STOPPED or ABORTED), the phase logic must upload the ACTUAL_AMOUNT and FEED_COMPLETE report parameters. The sign of the value in the ACTUAL_AMOUNT report parameter must match the configured feed type: Additions are positive or zero; Distributions are negative or zero. Deviating from this results in an error and the batch being HELD.
  • The Automatic Upload/Download functionality can be used to meet this protocol requirement. When used, the AMOUNT parameter downloads by the
    FactoryTalk Batch
    Server before the phase starts and the ACTUAL_AMOUNT and FEED_COMPLETE report parameters uploads after the phase logic runs to a terminal state. This simplifies the writing of phase logic.
    IMPORTANT:
    Uploading data into the material database has two constraints:
    • Some fields are only editable at configuration time. Only fields that may be changed at runtime will support uploading values.
    • Security may limit the set of users allowed to modify the database. The
      FactoryTalk Batch
      Server service must have adequate permissions to store to the material database.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal