Set project directories

Set directories for the following: Event Journal, Duplicate Journal, Error Logging, Instructions (if you are using
FactoryTalk®
e
Procedure®
), and Equipment Database.
IMPORTANT:
The
Event Journal
path must be defined or the
FactoryTalk Batch
Server will not start. The recommended
Event Journal
path is a subdirectory in the
FTBATCH_PROJECTS
share. In addition, if the
Event Journal
or
Duplicate Journal
path is invalid, the server will not start. If an invalid path is used, an error message indicating the invalid path is written to the
batchsvr.log
file.
To set project directories
  1. Open
    FactoryTalk Administration Console
    and sign in to the
    FactoryTalk
    Network Directory.
  2. In
    FactoryTalk Administration Console
    Explorer
    , do one of the following:
    • For a new
      FactoryTalk Batch
      Server, right-click the application or the area name and select
      Add New Server
      FactoryTalk Batch Server
      .
    • For an existing
      FactoryTalk Batch
      Server, expand the application or the area name, right-click the server, and select
      Properties
      .
  3. In the
    FactoryTalk Batch Services Properties
    dialog, select the
    Project Settings
    tab.
  4. In the
    Server
    box, select a server.
  5. In the
    Server directories
    area, for the
    Project path strategy
    :
    • Select
      Default paths
      to automatically populate project directories with paths from the
      Project path root
      directory.
    • Select
      Custom paths
      to browse to or enter paths for the project directories.
  6. Perform one of the following:
    • To save all changes, select
      Apply
      .
    • To save all changes and close the
      FactoryTalk Batch Services Properties
      dialog, select
      OK
      .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal