FactoryTalk Batch Services Properties dialog—primary server settings on the Project Settings tab

In the
FactoryTalk Batch Services Properties
dialog, use the
Project Settings
tab to configure the project paths.

Project Settings tab

Once you select a
FactoryTalk Batch
Server on the
Project Settings
tab, you can define the project paths and restart properties for that server.
TIP: For more information on configuring this tab for a secondary
FactoryTalk Batch
Server, see FactoryTalk Batch Services Properties dialog—secondary server settings on the Project Settings tab.
General settings
Setting
Description
Server
Select
Primary
to configure primary
FactoryTalk Batch
project settings. Valid values in the
Server
list include the following:
  • Primary
  • Secondary
    TIP: If, on the
    Secondary Server
    tab, the
    Enable secondary FactoryTalk Batch Server
    option is not selected, the secondary
    FactoryTalk Batch
    Server's data shows on the
    Project Settings
    tab but is not accessible.
Machine name
This read-only field shows the label for the primary
FactoryTalk Batch
Server, which comes from the
Computer hosting the primary FactoryTalk Batch Server
field explained in the section FactoryTalk Batch Services Properties dialog—General tab.

Server directories

The
Server directories
area is where you will define the project paths that the primary
FactoryTalk Batch
Server needs to access both its own directories and those of the paired secondary
FactoryTalk Batch
Server.
When you open the
Project Settings
tab, a message shows at the bottom of the
Project Settings
tab to alert you if any path is not visible from the current computer. For example:
The following paths do not exist: Project path root, Event Journal, Restart, Error logging, Instructions, Area Model, Recipe Directory
.
The table below defines the two
Project path strategy
options for configuring project paths. The option you select for the primary
FactoryTalk Batch
Server is independent of the option you select for the secondary
FactoryTalk Batch
Server.
Project path strategies
Strategy
Description
Default paths
When selected, the system disables the following fields and automatically populates them with a path that begins with the
Project path root
:
  • Event Journal
    :
    Project path root
    \journals\
  • Error logging
    :
    Project path root
    \logs\
  • Instructions
    :
    Project path root
    \instructions\
  • Restart
    :
    Project path root
    \restart\
  • Recipe Directory
    :
    Project path root
    \recipes\
Custom paths
When selected, all path fields are accessible for you to browse to or enter a path.
TIP: When switching from
Default paths
to
Custom paths
, the
Event Journal
,
Error logging
,
Instructions
,
Restart
, and
Recipe Directory
paths will all initially retain the default paths.
Project root directories
Directory
Description
Project path root
Browse to or enter the path to the location where you want to store your project directories.
If the location that you select is empty or invalid, the
FactoryTalk Batch
system will try to populate this field with the
FTBATCH_PROJECTS
directory. If the
FTBATCH_PROJECTS
directory does not exist, the system will then populate this field with the
C:\Users\Public\Documents
directory.
Area Model
Browse to or enter the path to the area model file (for example,
\\MY_COMPUTER\FTBATCH_PROJECTS\SampleDemo1\Recipes\ice_cream1.cfg
).
Project directories
Directory
Description
Event Journal
If you selected
Default paths
as the
Project path strategy
, this field is automatically populated. If you selected
Custom paths
, browse to or enter the path to the location where you want to store the
Event Journal
.
TIP:
You must define the
Event Journal
path or the primary
FactoryTalk Batch
Server will not start. The recommended
Event Journal
path is a subdirectory in the
Project path root
(for example,
FTBATCH_PROJECTS
).
The server will also not start if the
Event Journal
path is invalid. An error message indicating the invalid path appears in the
batchsvr.log
file.
Duplicate Journal
Browse to or enter the path to the location where you want to store the optional
Duplicate Journal
.
TIP: The primary
FactoryTalk Batch
Server will not start if the
Duplicate Journal
path is invalid. An error message indicating the invalid path appears in the
batchsvr.log
file.
If a secondary
FactoryTalk Batch
Server is configured, the recommended practice is to mirror the
Event Journal
and
Duplicate Journal
directories. For example:
  • The primary
    FactoryTalk Batch
    Server's
    Event Journal
    directory is the secondary
    FactoryTalk Batch
    Server's
    Duplicate Journal
    directory.
  • The primary
    FactoryTalk Batch
    Server's
    Duplicate Journal
    directory is the secondary
    FactoryTalk Batch
    Server's
    Event Journal
    directory.
Error logging
If you selected
Default paths
as the
Project path strategy
, this field is automatically populated. If you selected
Custom paths
, browse to or enter the path to the location where you want to store
Error logging
.
Instructions
If you selected
Default paths
as the
Project path strategy
, this field is automatically populated. If you selected
Custom paths
, browse to or enter the path to the location where you want to store
Instructions
.
TIP: This field is only accessible if, from the
General
tab, you selected the
Enable FactoryTalk eProcedure
option.
Restart
If you selected
Default paths
as the
Project path strategy
, this field is automatically populated. If you selected
Custom paths
, browse to or enter the path to the location where you want to store the files containing restart information.
TIP:
You must define a valid
Restart
path or the primary
FactoryTalk Batch
Server will not start and an error record writes to both
FactoryTalk
Events and the
batchsvr.log
file.
The server will also not start if the
Restart
path is invalid.
Duplicate Restart
Browse to or enter the path to the location where you want to store the files containing duplicate restart information. This directory is optional.
TIP: If the
Duplicate Restart
path is invalid, the primary
FactoryTalk Batch
Server will not start and an error record writes to both
FactoryTalk
Events and the
batchsvr.log
file.
If a secondary
FactoryTalk Batch
Server is configured, the recommended practice is to mirror the
Restart
and
Duplicate Restart
directories. For example:
  • The primary
    FactoryTalk Batch
    Server's
    Restart
    directory is the secondary
    FactoryTalk Batch
    Server's
    Duplicate Restart
    directory.
  • The primary
    FactoryTalk Batch
    Server's
    Duplicate Restart
    directory is the secondary
    FactoryTalk Batch
    Server's
    Restart
    directory.
Recipe storage settings
Setting
Description
Recipe format
Select the file format of stored recipes:
  • Binary file
    —Store recipes in separate files according to the recipe level and in a specified directory. Store procedures as
    .bpc
    files, unit procedures as
    .upc
    files, and operations as
    .uop
    files. This is the default value.
  • Microsoft SQL Server Database
    —Store recipes in a Microsoft SQL Server Database. This option enables the
    Database
    field.
  • XML file
    —Store recipes in separate
    .xml
    files. Store procedures as
    .pxml
    files, unit procedures as
    .uxml
    files, and operations as
    .oxml
    files.
Recipe Directory
If you selected
Default paths
as the
Project path strategy
, this field is automatically populated. If you selected
Custom paths
, browse to or enter the path to the location where you want to store the
Recipe Directory
.
Database
Lists available Microsoft SQL Server Databases. Select the database where you want to store recipes. Only enabled when you select
Microsoft SQL Server Database
as the
Recipe format
.
TIP: This field is only accessible when you select
Microsoft SQL Server Database
as the
Recipe format
option.

Server directories—Restart properties

The
Restart properties
area allows you to specify a method for restarting the primary
FactoryTalk Batch
Server when the Batch service is started from outside of the Batch Service Manager (for example, a computer reboot or using the Microsoft Windows Service Manager).
Restart properties
Setting
Description
Restart type
Select a restart method:
  • Cold Restart
    The
    FactoryTalk Batch
    Server starts in a new instance without restoring data from its previous run. Batches are not added back to the batch list, and operator arbitration states are not recovered. For all batches that were not restored, batch completion events are recorded in the
    FactoryTalk Batch
    Event Journals. After a Cold Restart, you will not be able to resume execution of batches from the previous instance. If Security Authority is enabled, SAIs in a secured area model and any secured recipes must match the current Network FactoryTalk Directory SAI.
  • Warm Restart
    Restarts the
    FactoryTalk Batch
    Server and attempts to restore the set of batches that were on the batch list when the server previously stopped. Batch complete events are added to the
    FactoryTalk Batch
    Event Journals for all batches that were not restored to the batch list. After a Warm Restart, any batches that are not restored cannot be recovered or resumed in the future. Batches are restored in Manual execution mode with active transitions in a HELD state. No validation for Security Authority is performed.
  • Warm All Restart
    The
    FactoryTalk Batch
    server attempts to restart but will not restart if it is unable to restore all the batches to the batch list. If a Warm All Restart attempt fails, the ability to restore batches in the future is not affected. After the issues are resolved, another attempt to restore the batches to the batch list can be made using Warm Restart, Warm All Restart, or Hot Restart. This is the default setting for automatic restarts. Batches are restored in Manual execution mode with active transitions in a HELD state. No validation for Security Authority is performed.
  • Hot Restart
    Follows all the startup rules of Warm All Restart. In addition, the
    FactoryTalk Batch
    Server attempts to restore batches to their last known state, including transition states and recipe modes, without any operator interaction.
Maximum wait for good controller communications during Hot Restart (sec)
Because a
Hot Restart
can run quickly, a communication failure can occur if the secondary
FactoryTalk Batch
Server does not have enough time to establish good communication with all data servers. You can configure this field to allow more time (in seconds) for establishing good communication on every area model in all data servers.
This field has a minimum integer value of 30 and a maximum integer value of 300. The default value is
60
sec.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal