Predictive Maintenance view
The Predictive Maintenance view displays predictive maintenance data for the contractors.
Predictive Maintenance data is only available when the device is online with the controller and when the identity data matches the configured project.
The options in this table describe the predictive maintenance parameters.
Parameter | Option |
|---|---|
View as | A display filter that displays predictive maintenance data according to the selected option:
|
Type | This control shows the type of the device from Component Group:
|
Status | Values are:
|
Remaining life/Elapsed life/Consumed life % | Depending on the selection in View as, displays:
|
Location | Identifies the location of the component within a product, device, or subsystem. |
Catalog number | Displays the replacement catalog number for the component. |
Reset | Resets the predictive maintenance data.
WARNING:
This action cannot be undone and may affect all subsequent PM data.
|
Settings | Displays the predictive maintenance settings dialog box. |
Refresh | Manually refreshes the predictive maintenance data when online with the device. |
Label | Description |
|---|---|
Refresh | Manually refreshes PM data in the view when online with the device. When the button is selected, the AOP reads PM data from the device by using the CIP explicit messages. |
Reset | Resets the predictive maintenance data. |
Settings | Displays the Predictive Maintenance Settings view. |
Provide Feedback