Predictive Maintenance settings
The Predictive Maintenance settings display options to set indicators and messages, and configures the alarm for the remaining life threshold percentage.
Parameter | Description |
|---|---|
Predicted life | Displays the Maximum life and the Remaining life threshold. |
Alarm | Displays the alarm notification settings selected by the user. |
Remaining life threshold % | Sets the remaining life alarm threshold for as the percentage of Maximum life. Values allowed:
TIP:
Remaining life varies according to selected threshold values.
|
Remaining life threshold | Displays the "Remaining life threshold", calculated by the settings view in the actual operations. |
Maximum life | Displays the "Maximum life". |
Custom percentage | When a Custom percentage is selected, enter a value for the Remaining life threshold. Allowed values are from 0% to 100.000%, in .001% increments. For example: When a 10% value is entered, the user may receive an alarm when 90% of useful product life is consumed. |
Enable operations alarm | Enables an alarm if remaining life is below threshold. If not enabled, the alarm will not trigger even if the threshold limit is crossed. If disabled, it hides the other configuration settings for "Operations". |
Enable operating hours alarm | Enables an alarm if remaining life is below threshold. If not enabled, alarm will not trigger even if the threshold limit is crossed. If disabled, hides the other configuration settings for "Operating hours". |
Cancel | Window closes without saving changes. |
Provide Feedback