Online Values

This view is shown for all types of starters/contactors (Non-Reversing Starter and Reversing Starter).

Refresh

The view header displays the type of starter/contactor. The window displays:
Select
Refresh
each time you need to check the status. The Online Values screen does not refresh automatically.
Refresh
refreshes the Online Values screen.

Status indicators

The statuses of Starter, Local Input, and HOA are shown using the following activity status indicators.
Activity status indicators
Status indicator
Description
Data read from the device indicates active status. For example, Starter is active in the forward direction or Interlock is active.
Data read from the device does not indicate active status. For example, Starter is not active in the forward direction.
Data read from the device indicates an error condition. For example, the interlock signal is inactive.
Data read from the device indicates that a warning condition exists.
No icon
When the trip/warning is disabled, the status icon is not displayed and the respective trip/warning text is grayed.

View header

The view header displays the name of the view and the type of device selected.
View header and device type
Device type
Header display
100-E-INT-X EtherNet/IP in-cabinet Non-Reversing Starter Interface
Online Values
104-E-INT-X EtherNet/IP in-cabinet Reversing Starter Interface
Online Values

Starter column

This column indicates the current status of the motor starter.
Starter and device type
Device type
Starter column display
100-E-INT-X EtherNet/IP in-cabinet Non-Reversing Starter Interface
Forward
104-E-INT-X EtherNet/IP in-cabinet Reversing Starter Interface
Forward or Reverse Depends on the read value

Local Input column

The indicator in this column indicates the status of the interlock input.
Local input and device type
Device type
Local Input column display
100-E-INT-X EtherNet/IP in-cabinet Non-Reversing Starter Interface
Interlock
104-E-INT-X EtherNet/IP in-cabinet Reversing Starter Interface
Interlock

HOA Status column

The indicator in this column indicates the status of Hand/Off/Auto mode. This column is visible only if, for the selected device,
Controlled By
is set to
Controller/Peer 2-Wire
or
Controller/Peer 3-Wire
mode.
HOA status and device type
Device type
HOA Status column display
100-E-INT-X EtherNet/IP in-cabinet Non-Reversing Starter Interface
  • Hand
  • Off
  • Auto
104-E-INT-X EtherNet/IP in-cabinet Reversing Starter Interface
  • Hand
  • Off
  • Auto
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal