Good Read Condition view parameters
The
Good Read Condition
view includes these parameters:Condition | Value |
|---|---|
Count of RFID tags in field is out of range | Enter Min and Max count. Min default is 1. Max default is 2. |
RFID tag read data matches command request data in output tag | Select the checkbox. |
RFID tag identifier matches identifier in output tag | Select the checkbox. |
Received signal strength indicator (RSSI) is in range | Enter Min and Max range. |
Signal strength is above the limit (difference from maximum RSSI) | Enter Limit. |
Provide Feedback