Good Read Condition view
Select the options to determine a valid read condition:
- Count of RFID tags in field is out of range
- RFID tag read data matches command request data in output tag
- RFID tag identifier matches identifier in output tag
- Received signal strength indicator (RSSI) is in range
- Signal strength is above the limit (difference from maximum RSSI)
Provide Feedback