Channel X - Modbus Slave view parameters

The
Channel
X
- Modbus Slave
view defines the characteristics of the Modbus Slave.
The
Channel
X
- Modbus Slave
view includes these parameters:
Parameter
Description
Modbus Format
Determines whether the Modbus transmission format is
Modbus RTU
or
Modbus ASCII
.
The default is Modbus RTU.
Inter-Frame Timeout
Specifies maximum delay time to receive data for the Remote Terminal Unit (RTU).
Tip: This parameter is available only when
Modbus Format
is set to
Modbus RTU
.
Node Address
Specifies the node address of the slave.
Valid value is from 1 through 247. The default is 1.
Diagnostics
When online, opens the diagnostics dialog box to view diagnostic counters for performance and error management with Channel X - Modbus Slave.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal