Channel X - Modbus Slave view
Use the
Channel
view to configure the Modbus Slave.X
- Modbus SlaveUse the
Channel
view to:X
- Modbus Slave- Select whether the Modbus transmission format isModbus RTUorModbus ASCII.
- Enter theInter-Frame Timeoutfor theModbus RTU.
- Enter theNode Addressof the slave device.
- Open the diagnostic dialog box to diagnose a communication problem with the Modbus Slave.
The
Channel
view is available when X
- Modbus SlaveChannel
in X
Device definition
is set to Modbus Slave
.Provide Feedback