Test Output Points view parameters (5034-IB8S)
The
Test Output Points
view includes these parameters:
Parameter | Description |
|---|---|
Point | Displays the point number to which this configuration
applies. |
Point Mode | Defines the mode of the test output point.
|
Diagnostics | Opens the Diagnostics dialog, which contains diagnostic
information. |
Provide Feedback