Test Output Points (Safety Input Modules)
Use
Test Output Points
to view or configure the points for the device.
TIP:
- TheTest Output Pointsview is only available if you choose 'This Controller' for the Configured By parameter on the Module Definition dialog.
- You must configure each point to use it in a Safety application. The test outputs are disabled by default.
Provide Feedback