Input Events view

Use
Input Events
to:
  • View a summary of the events configured for the device. Parameters are not editable on
    Events
    , but can be configured using the Tag Editor.
  • Access
    Input Eventxx
    where you can view parameters for a specific event.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal