Servers view parameters

Parameter
Description
Enable
Enables or disables the port by selecting or clearing the checkbox.
Name
Displays the name of the port.
Port
Displays the port number.
Protocol
Displays whether the protocol is Transmission Control Protocol (TCP) or User Datagram Protocol (UDP).
Refresh
Retrieves and displays the latest values from the device.
Set
Writes pending edits to the device.
  • Writing data to the device interrupts the access to the device and the SNMP client or web browser. Ensure an interruption at this time is acceptable before proceeding.
  • This parameter is available only when there are pending edits and there is no communication error in the device profile.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal