Servers view
Use the
Servers
view to enable and disable the Transmission Control Protocol (TCP)
or User Datagram Protocol (UDP) ports that are used by the device when it acts as a
server. EtherNet/IP uses TCP/IP or UDP/IP for communication. If the device profile is
online to a configurable TCP or UDP server, use the settings to:- Enable or disable the port.
- View information about the TCP or UDP port.
- Refresh communication to obtain the latest port information from the device.
Provide Feedback