Input Events view parameters

Parameter
Description
Event
Shows the event number to which this configuration applies.
Enable event
Shows whether the corresponding event trigger is active. Events are triggered once conditions match the event definition.
Latch event
Shows what happens to the current event when a new event is received.
When this parameter is selected, events are latched until acknowledged. A new event is lost if the previous event has not been acknowledged.
When this parameter is not selected, new events overwrite old events.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal