Input Events view

Use the
Input Events
view to:
  • View a summary of the events configured for the input devices.
  • Access the
    Input EventXX
    view to view parameters for a specific event.
TIP:
For the
Input Events
view to appear, set
Connection
in the
Device Definition
dialog box to one of these values:
  • Data With Events
  • Data with Events and Ethernet Status
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal