Change device definition

In the
Device Definition
dialog box, use the
Overview
view to change the definition of a device.
Prerequisites
  • Verify that the parent controller of the device is offline.
To change the device definition
  1. On the tab for the device, select
    Overview
    .
  2. In the
    Overview
    view, select
    Device definition
    .
  3. In the
    Device Definition
    dialog box, configure the parameters as needed.
  4. Select
    OK
    to finalize the changes and exit the dialog box.
  5. In the apply changes dialog box, select
    Yes
    to update the appropriate values and return to the
    Overview
    view.
    Data is recovered from the previous definition settings or set to their default values, as appropriate. Configurations are updated, as required for the new device definition.
  6. Select
    OK
    to make the changes to the project.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal