Device Definition dialog box - Overview view parameters
TIP:
- The available parameters and values depend on the device being configured. Parameters and values that do not apply to the device are hidden.
- These parameters appear shaded in Run mode.
Parameter | Description |
|---|---|
Device type | Displays the type of device selected during device configuration. |
Change type | Changes the device type and revision. |
Name | Specifies the device name. The name must be IEC_61131 compliant. If an invalid character is entered in this field or if the name exceeds 40 characters, the software ignores the character. You cannot change the name when online. |
Description | Specifies the description for the device. If the description exceeds the maximum length of 512 characters, the software ignores any extra characters. |
Ethernet Address | Specifies the IP configuration for the device.
|
Series | Specifies the device series. This parameter is not available when online. |
Revision | Specifies the device revision. This value only displays the major revisions that are applicable to the selected device series.
This parameter is not available when online. |
Electronic keying | Specifies the electronic keying for the device. Electronic keying compares the device defined in your project to the installed device. If keying fails, a fault occurs. Valid values include:
For more detailed information on Electronic Keying, see Electronic Keying in Logix5000 Control Systems Application Technique, publication LOGIX-AT001. |
Points | Specifies the number of I/O channels to be configured. If you select 16, all the 16 channels must be configured. If you select 8, you have the option to configure only eight channels. Valid values include:
|
Connection | Determines these options for the configured device type:
Possible values include:
|
MAOC Compatible Data | Specifies whether the data is compatible with Motion Arm Output Cam (MAOC) instruction. If the data is not compatible with MAOC, you cannot use this device with MAOC instruction. Possible values include:
This parameter applies to devices with major revision 2. |
Timestamp | Specifies the timestamp point assignment.
|
Provide Feedback