ChX value over range

One of these error conditions occurs:
Condition
Solution
ChX high signal value over range.
Enter a valid value within the range.
Refer to Low limit and high limit for the limits.
ChX low signal value over range.
Enter a valid value within the range.
Refer to Low limit and high limit for the limits.
ChX program user defined value over range.
Enter a value within the high clamp and low clamp limits defined in the
Limits
view.
ChX fault user defined value over range.
Enter a value within the high clamp and low clamp limits defined in the
Limits
view.
ChX rate limit value over range.
Enter a value less than the maximum allowed value of 32767.
RTS value over range. Value = 'xx', Maximum value = 'yy'.
Enter a value less than the maximum value allowed.
ChX rate alarm value over range. Value = 'xx', Minimum value = 'yy'.
Enter a value less than the maximum value allowed.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal