Motion Arm Registration (MAR)
This information applies to the
CompactLogix
5370, ControlLogix
5570, Compact GuardLogix
5370, GuardLogix
5570, Compact GuardLogix
5380, CompactLogix
5380, ControlLogix
5580, GuardLogix
5580, and ControlLogix 5590 controllers. Controller
differences are noted where applicable.Use the Motion Arm Registration (MAR) instruction to arm registration event checking for the specified axis. When the instruction is called, a registration event is armed based on the selected Registration Input and the specified Trigger Condition. When the specified Registration Input transition satisfies the Trigger Condition, the axis computes the axis position at the moment the event occurred based on hardware latched encoder count data and stores it in the associated Registration Position variable in the axis data structure. Also, the instruction’s Event (PC) bit is simultaneously set, as well as the Registration Event Status bit in the axis data structure. If Windowed Registration is selected, only registration events whose computed registration position falls within the Max and Min Position window are accepted. If the Registration Position falls outside this window the registration event checking is automatically rearmed.
Architecture | Standard | Safety |
---|---|---|
CompactLogix 5370, ControlLogix 5570, Compact GuardLogix 5370, and GuardLogix 5570 controllers | Yes | No |
Compact GuardLogix 5380, CompactLogix 5380, ControlLogix 5580, GuardLogix 5580,
and ControlLogix 5590 controllers | Yes | No |
Available Languages
Ladder Diagram

Function Block
This instruction is not available in function block.
Structured Text
MAR(Axis,MotionControl, TriggerCondition, WindowedRegistration, MinimumPosition, MaximumPosition, InputNumber);
Operands
Ladder Diagram
Operand | Type CompactLogix 5370, Compact GuardLogix 5370, Compact GuardLogix 5380, CompactLogix 5380 | Type ControlLogix 5570, GuardLogix 5570, ControlLogix
5580, GuardLogix 5580, and ControlLogix 5590 controllers | Format | Description |
Axis | AXIS_CIP_DRIVE | AXIS_CIP_DRIVE AXIS_SERVO AXIS_SERVO_DRIVE AXIS_GENERIC_DRIVE AXIS_GENERIC
TIP:
AXIS_GENERIC is supported by the
ControlLogix 5570 and the GuardLogix 5570 controllers
only. | Tag | Name of the axis on which to perform operation. For controllers that support the
REF_TO motion data types, the supported axis operand type can be replaced by an
equivalent REF_TO type. |
Motion Control | MOTION_INSTRUCTION | MOTION_INSTRUCTION | Tag | Structure used to access instruction status parameters. |
Trigger Condition | BOOLEAN | BOOLEAN | Immediate | Defines the Registration Input transition that defines the registration event. Select either: 0 = trigger on positive edge 1 = trigger on negative edge. |
Windowed Registration | BOOLEAN | BOOLEAN | Immediate | Enable (1) if registration is to be Windowed, that is, that the computed Registration Position must fall within the specified Min and Max Position limits to be accepted as a valid registration event. Select either: 0 = disabled 1 = enabled. |
Minimum Position | REAL | REAL | Immediate or Tag | Used when Windowed Registration is enabled. Registration Position must be greater than Min. Position limit before registration event is accepted. |
Maximum Position | REAL | REAL | Immediate or Tag | Used when Windowed Registration is enabled. Registration Position must be less than Max. Position limit before registration event is accepted. |
Input Number | SINT, INT, or DINT | SINT, INT, or DINT | 1 or 2 | Specifies the Registration Input to select. 1 = Registration 1 Position 2 = Registration 2 Position. |
See Structured Text Syntax for
more information on the syntax of expressions within structured text.
For the operands that require you to select from available options, enter your selection as:
This Operand | Has These Options Which You | |
Enter as Text | Or Enter as a Number | |
TriggerCondition | positive_edge negative_edge | 0 1 |
WindowedRegistration | disabled enabled | 0 1 |
MOTION_INSTRUCTION Structure
Mnemonic | Description |
.EN (Enable) Bit 31 | It is set to true when the rung makes a false-to-true transition and remains set until the servo message transaction is completed and the rung goes false. |
.DN (Done) Bit 29 | It is set to true when the axis registration event checking has been successfully armed. |
.ER (Error) Bit 28 | It is set to to true to indicate that the instruction detected an error, such as if you specified an unconfigured axis. |
.IP (In Process) Bit 26 | It is set to true on positive rung transition and cleared to false after the registration event has occurred, or has been superseded by another Motion Arm Reg command, or terminated by a Motion Disarm Reg command. |
.PC (Process Complete) Bit 27 | It is set to true when a registration event occurs. |
Description
The MAR instruction sets up a registration event to store the actual positions of the specified physical axis on the specified edge of the selected dedicated high speed Registration input for that axis.
When an MAR instruction is executed, the RegEventStatus bit is set to 0 (FALSE) and the selected Registration input for the specified axis is monitored until a Registration input transition of the selected type (the registration event) occurs. When the registration event occurs, the RegEventStatus bit for the axis is set to 1 (TRUE) and the Actual Position of the axis is stored in the Registration Position variable corresponding to the registration input (for example, Registration 1 Position 1 or Registration 2 Position).
Registration

Multiple registration events may be active at any time for a given axis, but only one may be active per registration input. Each event is monitored independently and may be checked using the appropriate RegEventStatus bit.
Windowed Registration
When the Windowed Reg checkbox is checked, the selected trip state only results in a registration event if it occurs when the axis is within the window defined by the minimum and maximum positions as shown below.

Enter values or tag variables for the desired absolute positions that define the position window within which the selected trip state of the Registration input is valid. Windowed registration is useful in providing a mechanism to ignore spurious or random transitions of the registration sensor, thus improving the noise immunity of high-speed registration inputs.
For linear axes, the values can be positive, negative, or a combination. However, the Minimum Position value must be less than the Maximum Position value for the registration event to occur. For rotary axes, both values must be less than the unwind value set in the motion controller’s machine setup menu. The Minimum Position value can be greater than the Maximum Position value for registration windows that cross the unwind point of the axis, as shown below.
Position Window for Rotary Axis

Rearming an MAR Instruction
If your application requires rapid and continuous detection of a registration sensor, we recommend using this logic:
Ladder Logic for Continuous Registration Detection

To rearm the MAR instruction, the rung must change from false to true. The rate at which this logic functions depends on:
- program scan time
- motion task coarse update rateIMPORTANT: In large I/O connections, force values can slow down the rate at which the controller processes repetitive motion registration.
To successfully execute a MAR instruction, the targeted axis must be configured as either a Servo or Feedback Only axis. Otherwise, the instruction errs.
IMPORTANT:
The instruction execution may take multiple scans to execute because it
requires multiple coarse updates to complete the request. The Done (.DN) bit is not set
immediately, but only after the request completes.
In this transitional instruction, the relay ladder, toggle the Rung-condition-in from cleared to set each time the instruction should execute.
Affects Math Status Flags
No
Major/Minor Faults
None specific to this instruction. A major fault can occur if an uninitialized reference or
a reference of incorrect type is passed to the Axis Operand. See Common Attributes for operand-related faults.
Execution
Ladder Diagram
Condition/State | Action Taken |
Prescan | The .EN, .DN, .ER, and .IP bits are cleared to false. |
Rung-condition-in is false | The .EN bit is cleared to false if either the .DN or .ER bit is true. |
Rung-condition-in is true | The .EN bit is set to true and the instruction executes. |
Postscan | N/A |
Structured Text
Condition/State | Action Taken |
Prescan | See Prescan in the Ladder Diagram table. |
Normal execution | See Rung-condition-in is false, followed by rung is true in the Ladder Diagram table. |
Postscan | See Postscan in the Ladder Diagram table. |
Error Codes
See Motion Error Codes .ERR for Motion
Instructions.
Extended Error Codes
Extended Error Codes provide additional instruction specific information for the Error
Codes that are generic to many instructions. The following Extended Error codes help to
pinpoint the problem when the MAR instruction receives a Servo Message Failure (12) error
message. See Motion Error Codes .ERR for Motion
Instructions.
Associated Error Code (decimal) | Extended Error Code (decimal) | Meaning |
SERVO_MESSAGE_FAILURE (12) | No Response (2) | Not enough memory resources to complete request. (SERCOS) |
SERVO_MESSAGE_FAILURE (12) | Invalid value (3) | Registration input provided is out of range. |
SERVO_MESSAGE_FAILURE (12) | Device in wrong state (16). | Redefine Position, Home, and Registration 2 are mutually exclusive. (SERCOS) |
Extended Error codes for the Parameter Out of Range (13) error code work a little differently. Rather than having a standard enumeration, the number that appears for the Extended Error code refers to the number of the operand as they are listed in the faceplate from top to bottom with the first operand being counted as zero. Therefore for the MAR instruction, an extended error code of 4 would refer to the Min Position value. You would then have to check your value with the accepted range of values for the instruction.
Status Bits
MAR Changes to Status Bits
Bit Name | State | Meaning |
RegEvent1ArmedStatus RegEvent2ArmedStatus | TRUE | The axis is looking for a registration event. |
RegEvent1Status RegEvent2Status | FALSE | The previous registration event is cleared. |
Example
Ladder Diagram

Structured Text
MAR(Axis1, MAR_2, Positive_Edge, enabled, minmarpos_1, maxmarpos_1, 1);
Provide Feedback