Motion Event Instructions

These are the motion event instructions.
Available Instructions
Ladder Diagram and Structured Text
Function Block
Not available
IMPORTANT: Tags used for the motion control attribute of instructions should only be used once. Reuse of the motion control tag in other instructions can cause unintended operation. This may result in damage to equipment or personal injury.
Motion event instructions control the arming and disarming of special event checking functions, such as registration and watch position.
The motion event instructions are:
If you want to:
Use this instruction:
Arm watch-position event-checking for an axis.
MAW
Disarm watch-position event-checking for an axis.
MDW
Arm servo-module registration-event checking for an axis.
MAR
Disarm servo-module registration-event checking for an axis.
MDR
Arm an Output Cam.
MAOC
Disarm an Output Cam
MDOC
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal