Publish a library object
Publish a library from an ACD repository to an ACM repository or a folder repository by copying the library from the tree node to the required repository node. Copy existing library objects from one repository to another for collaboration or to restore from a backup.
To publish a library object from the ACD repository to a folder repository or the ACM database
- Select the library object in the ACD Repository and drag it on top of the icon for the folder repository or ACM database.TIP:The pointer changes to the "unavailable" icon until the pointer is over a valid repository icon.The Library Import Configuration dialog box opens.IMPORTANT:When publishing into the ACM database the new library object will be compared to all library objects with the same catalog number that are currently stored in the ACM database, and many of the items in theLibrary Import Configurationdialog box will be completed using the information from the ACD or ACM database. Information that originates from the ACD cannot be edited in theLibrary Import Configurationdialog box.If publishing the library results in duplicated names, a warning message is displayed. ClickOKto proceed with publishing and accept the duplicate names.
- Enter the information for the library object.
- ClickOKto add the library object to the repository.
Provide Feedback